为 AI 处理器供电——48V 垂直供电重塑行业格局
AI 模型需要巨大的电流,导致传统多相设计超过 50 相 —— 从而引发空间、散热和控制方面的限制,Vicor 针对这些问题提供了解决方案
Density of power components has increased several orders of magnitude over the past couple of decades. On one hand this has led to a significant reduction in size and cost of power electronic converters; on the other hand, designing the appropriate cooling solution has become more and more challenging. In many cases, thermal management is the gating item that determines the feasibility of a project, and the thermal management solutions need to be evaluated at a very early stage in the design of a power supply.
To simplify your thermal evaluation Vicor has released several simulation models that enable evaluation of the thermal characteristics of our products. The simulator allows you to do a preliminary evaluation of the functionality of our products in your specific environment and operating conditions. The simulator evaluates whether the operating conditions selected by the user when under the selected cooling option are within specification, or if modification to the selected cooling strategy are needed.Overview of Vicor thermal simulator interface. In this example, the cooling type selected was “Heat Sink”. The Option of a “User Defined Cold Plate” is also available.
With just a few clicks, you can select the Vicor power component you are planning to use, customize your source and load conditions, ambient temperature, and evaluate the feasibility under several possible choices of cooling solutions. These solutions may include various types of Vicor heatsinks, as well as custom defined cold plate solutions. In a few seconds you will be able to determine the ideal cooling approach for your project, and you can proceed with your design knowing that thermal management has been addressed already!
Figure 2: Examples of results returned by the thermal simulation: the top image shows a cooling solution that is adequate for the selected operating conditions; the bottom one shows a cooling solution that is undersized, and provides directions on how to improve the thermal management.
为 AI 处理器供电——48V 垂直供电重塑行业格局
AI 模型需要巨大的电流,导致传统多相设计超过 50 相 —— 从而引发空间、散热和控制方面的限制,Vicor 针对这些问题提供了解决方案
创新的 48V AI 电源架构,兼顾高电流密度与高电流增益
Vicor 48V 分比式电源架构大幅降低了热损耗并提供高电流密度,满足 AI 处理器的极端功率需求
为 AI 供电,48V 分比式电源架构™ 大幅降低热损耗,性能优于多相方案
AI 硬件面临着严峻的功率与散热限制。工程师们对 48V 与 6V 中间母线以及新的垂直供电(VPD)结构进行讨论
Betterfrost:精准加热,高效除冰
Betterfrost 使用 48V 模块进行脉冲传导玻璃加热,可在 80 秒内去除冰层,同时将启动除霜能量降低 95%